Conclusion - Metasys - LIT-12011549 - Supervisory Device - LCS85 Controller - 12.0

LCS85 Product Bulletin

Product
Controls > Supervisory Controls > LCS85 Controller
Document type
Product Bulletin
Document number
LIT-12011549
Version
12.0
Revision date
2022-05-04
Product status
Active

The LCS85 affirms Johnson Controls position as a leader in the BAS industry and as an innovator of solutions for the complete management of buildings. The integration of IT and Internet standards into the LCS85 platform, as well as the use of open protocols for field networks, bring the benefits of the global communications and control industries into one system. Web browser-based access from any location is key to the effective use of the automation network.

The Metasys system continues to be the integrating network within buildings and has now been extended to bridge the gap between traditional control systems and the business and communication network systems of the enterprise.

The LCS85 and Metasys web-enabled network are wise investments that yield returns to the building owner and operator far into the future.