Problem |
Solution |
---|---|
You receive the following error message when installing an LCS85:
|
Metasys SCT is installed on the computer. Click OK, and uninstall SCT on the computer. Once SCT is uninstalled, follow the steps in Installing LCS85 software to install the LCS85. |
You experience installation problems and would like to consult the error log. |
Error messages for installation problems are located here: C:\Users\<name_of_currently_logged_in_user>\AppData\Local Metasys_LonWorks_Control_Server_11.0_x.html, where x is a time/date stamp in the format YYYYMMDDHHMMSS. Example: Metasys_LonWorks_Control_Server_11.0_20180404112550.html |
You experience problems when upgrading your LCS85. |
Uninstall the previous version of LCS85 software. Follow these steps to resolve the issue:
|
During the upgrade procedure, the following error message appears and the progress bar does not advance:
|
The device manager service could not be deleted during the installation. Click OK to proceed with the installation. If you click OK and the upgrade does not progress, continue with these steps:
|