Inserting third-party integrations - Metasys - LIT-12011623 - Supervisory Device - LCS85 Controller - 11.0

LCS85 Installation and Upgrade Guide

Product
Controls > Supervisory Controls > LCS85 Controller
Document number
LIT-12011623
Version
11.0
Revision date
2020-10-30

Refer to the following documents for information about how to insert the following integrations:

  • KNX: Network Engine Commissioning for KNX Vendor Integration Application Note (LIT-12013148)
  • M-Bus: Network Engine Commissioning for M-Bus Vendor Integration Application Note (LIT-12013149)
  • Modbus: Network Engine Commissioning for Modbus Integration Application Note (LIT-12013150)
  • C•CURE-victor: Network Engine Commissioning for C•CURE-victor Integration Application Note (LIT-12013151)
  • OPC UA Servers: Metasys System Commissioning for OPC UA Integration (LIT-12013545)
    Note: The OPC UA integration is only available in Release 11.0.