Removing an existing software driver and driver components - Metasys - LIT-12011623 - Supervisory Device - LCS85 Controller - 11.0

LCS85 Installation and Upgrade Guide

Product
Controls > Supervisory Controls > LCS85 Controller
Document type
Installation Guide
Document number
LIT-12011623
Version
11.0
Revision date
2020-10-30

About this task

Important: If you are installing a driver upgrade over the existing driver, you can skip this section.

You must remove the existing software driver and driver components before you upgrade. To remove an existing driver and driver components, complete the following steps:

Procedure

  1. Go to Control Panel and browse to Programs > Programs and Features .
  2. After the list of programs appears, select each of the following programs and remove them individually:
    • Easylon EIA-852 Interface
    • Easylon RNI Client
    • Easylon WLDV32.DLL
    Note: If you need to remove more than one program, wait until one program is removed before you remove another one.
  3. Restart your computer after all programs are uninstalled.
  4. In the Control Panel, browse to System and Security > Administrative Tools and double-click Computer Management.
  5. In the left pane, click Device Manager in the tree.
  6. In the right pane, expand LON Adapters in the tree.
  7. For each item listed under LON Adapters, right-click the item and click Uninstall.
    Note: The Confirm Device Uninstall window may appear when you select an item to uninstall. Use this screen to uninstall all items listed under LON Adapters. Select the Delete the driver software for this device check box and click OK. If the screen does not appear, continue to uninstall each item listed one at a time.
  8. Restart your computer after you uninstall all items.
  9. Type wldv32.dll in the Search box of the Start screen.
  10. Right-click each file and click Delete.
    Important: Do not delete any files from the LCS85 installation package you copied to your server in the Installing LCS85 software section. The FUSE installer copies the installation files to C:\Program Files (x86)\Johnson Controls\LCS8520\11.0.0.8791\Easylon-WDM_V7.9.2005-Jci, where 11.0.0.8791 references the release that you install.