About this task
Important: If you are
installing a driver upgrade over the existing driver, you can skip this section.
Back up your LCS85 database before you upgrade your software driver. If you restart
the LCS after you remove the software driver, the process deletes the Metasys
LonWorks Integration information from the database. To prevent this issue and ensure
that you preserve your database, you must stop and disable the Metasys III Device
Manager service.
To stop and disable the Metasys Device III Manager service, complete the following steps: