During the LonWorks software driver upgrade you are prompted for certain information about your LCS85. If you have multiple LCS85s on your site, you must get the following information for each server:
-
Neuron ID
-
Media Access Control (MAC) address
-
LonWorks software driver license key
If you are unsure of any of these values, you can obtain this information through the Easylon IP Interface.
To obtain the required information for your driver upgrade, complete the following steps:
- In the Search box on the Start
screen, type
Config 852 Interface, then select Config 852 Interface from the Apps results. - Capture the entire Easylon Interface Config window and save it to an image file. You reference this screen capture when you install the new LonWorks software driver. See Installing and licensing a new LonWorks software driver.