Obtaining required information for driver upgrade - Metasys - LIT-12011623 - Supervisory Device - LCS85 Controller - 11.0

LCS85 Installation and Upgrade Guide

Brand
Metasys
Product name
LCS85 Controller
Document type
Installation Guide
Document number
LIT-12011623
Version
11.0
Revision date
2020-10-30
Language
English

During the LonWorks software driver upgrade you are prompted for certain information about your LCS85. If you have multiple LCS85s on your site, you must get the following information for each server:

  • Neuron ID

  • Media Access Control (MAC) address

  • LonWorks software driver license key

If you are unsure of any of these values, you can obtain this information through the Easylon IP Interface.

To obtain the required information for your driver upgrade, complete the following steps:

  1. In the Search box on the Start screen, type Config 852 Interface, then select Config 852 Interface from the Apps results.
  2. Capture the entire Easylon Interface Config window and save it to an image file. You reference this screen capture when you install the new LonWorks software driver. See Installing and licensing a new LonWorks software driver.