Procedure
-
Use Windows File Explorer to locate the following software
driver folder on your hard disk: C:\Program Files
(x86)\Johnson Controls\LCS8520\X.X.X.XXXX, where X corresponds to
the Metasys release and software build number.
The software driver folder is named Easylon-WDM_VX.X.XXXX-JCI, where X is the version number of the driver. For example, if you use version 7.9.2005, the software driver folder is named Easylon-WDM_V7.9.2005-JCI.
- In the software driver folder, open the Wldv32 folder.
-
Double-click
Setup.exe. -
Install the application in the default directory
C:\Easylon. - Restart your computer.
- Use Windows File Explorer to navigate back to the software driver folder C:\Program Files (x86)\JohnsonControls\LCS8520\X.X.XXXX\Easylon-WDM_VX.X.XXXX-JCI. Browse to the 852 Server folder.
- Double-click Setup.exe.
- Install the application in the default directory C:\EasyLon\852.
- Use the screen capture you created in Step 2 of Obtaining required information for driver upgrade and use the data in Table 1 to configure the values and options found in the Easylon IP Interface Config window.
- Click Apply.
-
Verify your changes are successful. If the changes are successful, the message
Successfully started 852 Interfaceappears in the Log field. - Close the Easylon IP Interface Config window.