Installing the new LonWorks software driver - Metasys - LIT-12011623 - Supervisory Device - LCS85 Controller - 11.0

LCS85 Installation and Upgrade Guide

Product
Controls > Supervisory Controls > LCS85 Controller
Document type
Installation Guide
Document number
LIT-12011623
Version
11.0
Revision date
2020-10-30

Procedure

  1. Use Windows File Explorer to locate the following software driver folder on your hard disk: C:\Program Files (x86)\Johnson Controls\LCS8520\X.X.X.XXXX, where X corresponds to the Metasys release and software build number.

    The software driver folder is named Easylon-WDM_VX.X.XXXX-JCI, where X is the version number of the driver. For example, if you use version 7.9.2005, the software driver folder is named Easylon-WDM_V7.9.2005-JCI.

  2. In the software driver folder, open the Wldv32 folder.
  3. Double-click Setup.exe.
  4. Install the application in the default directory C:\Easylon.
  5. Restart your computer.
  6. Use Windows File Explorer to navigate back to the software driver folder C:\Program Files (x86)\JohnsonControls\LCS8520\X.X.XXXX\Easylon-WDM_VX.X.XXXX-JCI. Browse to the 852 Server folder.
  7. Double-click Setup.exe.
  8. Install the application in the default directory C:\EasyLon\852.
  9. Use the screen capture you created in Step 2 of Obtaining required information for driver upgrade and use the data in Table 1 to configure the values and options found in the Easylon IP Interface Config window.
  10. Click Apply.
  11. Verify your changes are successful. If the changes are successful, the message Successfully started 852 Interface appears in the Log field.
  12. Close the Easylon IP Interface Config window.