Preparing an equipment definition in SCT - Metasys - LIT-12013961 - SE000200P - SE000100B - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active

You can download a Kaiterra equipment definition from the Global Library site: https://globallibrary.azurewebsites.net/#/equipmentdefinition. The equipment definition defines a selection of the available points in a Kaiterra sensor that are presented in the Metasys UI. The equipment definition is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Insert Equipment Definition section in the Metasys SCT Help (LIT-12011964).

  1. Download the equipment definition file from the Global Library, or create one in SCT.
  2. Launch the SCT, and then open an archive.
  3. In the All Items tree, expand the server object; for example the ADS, or ADX.
  4. Right-click the Equipment Definitions or Definitions folder, and then click Import Equipment Definition.
  5. Navigate to the location of the equipment definition you downloaded, select the file, then click Import.
  6. After the import is complete, a confirmation message appears. Click OK. The equipment definition imports and is listed under the Equipment Definitions folder.
Figure 1. Sensedge Mini Equipment Definition in SCT