Preparing a controller template in SCT - Metasys - LIT-12013961 - SE000200P - SE000100B - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active

You can download a Kaiterra controller template from the Global Library site: https://globallibrary.azurewebsites.net/#/controllertemplate. The controller template defines a set of points that are available in a Kaiterra sensor. The controller template is required if you use the Rapid Archive to complete the integration process. For more information, refer to the Controller Templates section in the Metasys SCT Help (LIT-12011964).

To import the controller template into an SCT archive, complete the following steps:

  1. Download the controller template file from the Global Library or create one in SCT.
  2. Launch the SCT, and then open an archive.
  3. In the All Items tree, expand the Configuration Data folder.
  4. Right-click the SCT Controller Templates folder, and then click Import Template.
  5. Navigate to the location of the controller template you downloaded, select the template, then click Import.
  6. After the import is complete, a confirmation message appears. Click OK. The controller template imports and is listed under the SCT Controller Templates folder.
Figure 1. Sensedge Mini Controller Template in SCT