Linking a controller template to an equipment definition in SCT - Metasys - LIT-12013961 - SE000100B - SE000200P - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active

After you import both the equipment definition and the controller template, you must create a link between them.

  1. Open the controller template in a focus window and select the Configuration tab.
  2. Click Edit.
  3. In the Definition Link parameter, click the browse icon to open the Select Item wizard.
  4. Navigate to the equipment definition and select it.
  5. Click OK.
  6. Click Save.