Integration with Metasys UI - Metasys - LIT-12013961 - SE000200P - SE000100B - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active

Use the Metasys UI to manage Kaiterra sensor information, monitor IAQ information, and view equipment sumaries. For information on using the Metasys UI, refer to the Metasys UI Help (LIT-12011953).

A wide variety of graphics are possible and a generic file is also available for download.

Figure 1. Example of a Kaiterra sensor in the Metasys UI