Completing the Kaiterra sensor schedule in Excel - Metasys - LIT-12013961 - SE000200P - SE000100B - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active

Enter the Kaiterra sensor name and BACnet instance numbers into a RAC schedule spreadsheet where you can continue to add more data, including space names, equipment names and references, Engine information, and the equipment definition and controller template names.

For detailed information on use of the Rapid Archive Schedule, refer to the Rapid Archive Schedule Population in the Rapid Archive Wizard section in the Metasys SCT: System Configuration Tool Help (LIT-12011964).