Requirements - Metasys - LIT-12013961 - SE000200P - SE000100B - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active
To integrate Kaiterra sensors over BACnet/IP to an Metasys Engine, you must have the following:
  • Commissioned and working Kaiterra sensor.
  • A properly installed and commissioned Metasys Engine from which to perform the BACnet/IP integration.
  • System Configuration Tool (SCT) Release 13.1 or later if using RAC.