Metasys Engines - Metasys - LIT-12013961 - SE000200P - SE000100B - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product
Sensors and Meters > Indoor Air Quality Sensors > Kaiterra Indoor Air Quality Sensor
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active
The Metasys Network Engines are web-enabled, IP-based supervisory devices that connect BAS networks to IP networks. An Engine can operate as a stand-alone site director or can be part of a larger network reporting to a Metasys server. You install the Johnson Controls Launcher application on a computer to access a Engine, and then monitor and control BAS devices and systems using the Engine or Metasys server user interfaces from a computer or mobile device. Refer to Launcher Help (LIT-12011742) for further information.
Figure 1. Metasys SNC and SNE Engines