Inserting field points - Metasys - LIT-12013961 - SE000100B - SE000200P - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Brand
Metasys
Product name
Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active
Language
English

If you are continuing from the Field Device Extension wizard above, proceed to Step 3 with Select Definition Mode.

  1. Drag the Kaiterra sensor object from the navigation panel to the display panel. The Focus tab for the device appears.
  2. Click Insert Field Point. The Insert Point wizard appears.
  3. In the Destination window, select the Kaiterra sensor if not already selected and click Next.
  4. In the Select Definition Mode window, click Invoke Auto Discovery to begin a BACnet point discovery.
  5. The Auto Detect Utility wizard appears. This wizard shows that a discovery is in progress. When the new points are discovered from the sensor, they appear in the discovery results list. Click Close when the discovery is complete. The Point Mapping wizard appears.
  6. Use the Point Mapping dialog to select the points you want to map.