Inserting a field device manually - Metasys - LIT-12013961 - SE000100B - SE000200P - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Brand
Metasys
Product name
Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active
Language
English
  1. Drag the BACnet/IP integration object from the navigation panel to the display panel. The Focus tab for the BACnet IP integration appears.
  2. Click Insert > Field Device. The Insert Field Device wizard appears.
  3. In the Destination window, select the BACnet IP integration if not already selected and click Next.
  4. In the Select Definition Mode window, click the Manual radio button, then select General BACnet Device. Click Next.
  5. In the Identifier window, enter a unique name for this device. Click Next.
  6. In the Configure window, select the Hardware tab and enter the expected Instance Number of the Kaiterra sensor.
  7. In the Summary window, click Finish. The Extension wizard appears.
  8. Click Done since we are not interested in adding extensions for the device.
  9. The Field Device Extension wizard appears. Click New and continue inserting field points as described in the next section, Inserting field points.