Appendix - Metasys - LIT-12013961 - SE000100B - SE000200P - Kaiterra Indoor Air Quality Sensor

Kaiterra Indoor Air Quality Sensor and Metasys Integration Guide

Product name
Kaiterra Indoor Air Quality Sensor
Document type
Integration Guide
Document number
LIT-12013961
Revision date
2021-12-03
Product status
Active

See the following table for the BACnet object list of Kaiterra sensors.

Table 1. Kaiterra Sensedge Mini BACnet point description

Point name

Description

CO2 The current value of carbon dioxide in ppm
Humidity The current value of relative humidity in %
KM200 Module Lifespan The estimated lifecycle remaining on the particulate matter module in percentage
KM203 Module Lifespan The estimated lifecycle remaining on the total organic volatile compound module in percentage
PM10 The current value of particulate matter of size < 10 µg/m3 in µg/m3
PM2.5 The current value of particulate matter of size < 2.5 µg/m3 in µg/m3
Sec Total runtime in seconds
TVOC The current value of total volatile organic compound in ppb
Temperature The current value of temperature in degree Celsius
Table 2. Kaiterra Sensedge BACnet point description

Point name

Description

CO2 The current value of carbon dioxide in ppm
Humidity The current value of relative humidity in %
PM10 The current value of particulate matter of size < 10 µg/m3 in µg/m3
PM2.5 The current value of particulate matter of size < 2.5 µg/m3 in µg/m3
TVOC The current value of total volatile organic compound in ppb
Temperature The current value of temperature in degree Celsius
TemperatureF The current value of temperature in degree Fahrenheit

Configure the Kaiterra sensor BACnet properties to ensure BACnet communications is successful and that Kaiterra sensors do not interfere with existing devices on the BACnet network. These settings are described in the following table.

Table 3. Kaiterra sensor BACnet settings

Setting

Description

Local Device ID

The BACnet device ID for this Kaiterra Sensedge Mini sensor. Set this Device ID to a value that does not conflict with other BACnet device IDs on the network or communication issues may occur.

The default value is empty which means BACnet is disabled.

BACnet UDP Port

The UDP port restricts BACnet communications to devices that have the same UDP port setting. This value must match the BACnet UDP port number set in the Engine you are integrating with or communication between devices cannot occur.

The default value of 47808 is a common value on most BACnet networks. However, make sure that you check this with the site’s BACnet network expert.