How do I add the Tooltip effect?
To add the Tooltip effect to a shape, symbol, element of a symbol, or an image:
- Click in the Behavior Name field to add a name. Click the tick button.
- Click
to select the Tooltip effect.
- Configure the Tooltip effect. Enter text in the Text
field. You can add up to 64 characters. Figure 1. Tooltip Effect
Click Next.
- Select a trigger. See Working with Triggers.
- Add a rule. Rules are optional unless a Value Change trigger is used for the Custom Behavior. See Working with Rules.
- Click SAVE.
Figure 2. Completed Tooltip Example

What are the use cases for using the Tooltip effect?
The Tooltip effect can be used to display text when hovering over a shape, symbol, element of a symbol, or image.
What can I apply the Tooltip effect to?
You can apply the Hide effect to any shape, symbol, element of a symbol, or image.