What is the Logic Viewer and Editor widget?
This widget provides a single view of Logic Connection Tool (LCT) logic diagrams in Metasys UI and JCT. LCT logic is required to control certain aspects of a Building Automation System (BAS). Program (Control System) objects are often used to create supervisory control logic to comply with the sequence of operations called out in project plans, specifications, or contract documents for various systems in a BAS.
The widget consists of a viewing component, hereafter called Logic Viewer, and an editing component, hereafter called Logic Editor.
The Logic Viewer provides a visual representation of supervisory LCT logic for you to understand, trace, and troubleshoot logic in the Metasys system. The Logic Editor provides the functionality to create new logic and edit existing logic.
Who can access the Logic Viewer and Editor? Who can modify logic diagrams?
You do not require special authorization or licensing to access the Logic Viewer and Editor and to modify logic diagrams.
How do I access the Logic Viewer and Editor?
What is the layout of the Logic Viewer and Editor?
| Number | Name | Description |
|---|---|---|
| 1 | Main display | Provides a single view of the logic diagram. The diagram displays live values in Metasys UI and not in JCT. |
| 2 | Export | Exports the logic diagram in PDF format. |
| 3 | Edit | Click to open the Logic Editor. |
| 4 | Select | Select an element of the logic diagram and navigate to it. |
| 5 | Pan | Move the entire logic diagram. |
| 6 | Zoom In | Zoom in to the logic diagram. You can also move the wheel button on your mouse to zoom in. |
| 7 | Zoom Reset | Zoom Reset fits a logic diagram in the main display. The zoom level is adjusted based on the content of the logic diagram. |
| 8 | Zoom Out | Zoom out of the logic diagram. You can also move the wheel button on your mouse to zoom out. |
| 9 | Reference block example | Input Reference blocks and Output Reference blocks provide information and links for their referenced object and configured attribute. See the following figures. |
|
Figure 2. Input Reference block with connection line shown
|
Figure 3. Output Reference block with connection line hidden
|
| Number | Name | Description |
|---|---|---|
| 1 | Global status indicator icon | Appears when live values are shown. Displays the same global status indicator icon as appears in the Network tree and Views for the referenced object. |
| 2 | Object type icon | Displays the object type icon for the referenced object. |
| 3 | Referenced object | Identifies the referenced object by displaying its name or item reference as a link to the object. |
| 4 | Trigger icon | Applies to only Input Reference blocks. A star icon appears when the block is configured with Trigger selected. |
| 5 | Connection value and priority | When live values are shown, the connection
value displays near the starting connection point. For hidden
connections, the value also displays at the ending connection
point. For priority connections, the configured priority displays at the ending connection point. For hidden connections, the priority also displays at the starting connection point. Note: Comparing
the connection value and priority to the current value shown
in an Output Reference block can help you identify cases
where the logic is currently not in control. For example, in
the previous figure, you can see that an Operator Override
is controlling the referenced object, and as a result, the
lower priority value from the logic cannot take
effect.
|
| 6 | Information icon | When clicked, displays a tooltip with additional information and links for the referenced object, such as the configured attribute and the item reference. For server sites that have Spaces and Equipment defined, the tooltip also includes space and equipment information. |
| 7 | Status color bars | Appears only when live values are shown. Displays colored bars to indicate the current status of the referenced object. The colors match the status colors configured on the Graphic tab in Site Settings. |
| 8 | Current value | Appears only when live values are shown. Lists the current value and units (if applicable) for the configured attribute. If the configured attribute is the referenced object’s Present Value or default attribute, the value appears as a link to open Commanding. |
| 9 | Current priority or configured attribute |
When live values are shown and the configured attribute for the block is Present Value, this area lists the referenced object's current command priority when applicable, and is blank if Present Value does not support command priorities or its Priority Array is empty. For all other cases, this area lists the name of the configured attribute. |
| Number | Name | Description |
|---|---|---|
| 1 | Logic Blocks pane | Select from a range of logic blocks to create or edit a logic diagram. Hover over a logic block to see the name of the logic block. See Which logic blocks are available and what do they do? for more details. |
| 2 | Logic canvas | The logic canvas provides the display area for the logic that is currently open. You add, move, and delete logic elements in this area to create your logic diagram. |
| 3 | Logic Checker | Check the logic you created to find out if there are any configuration warnings. Hover over the relevant block or exclamation points to learn more about the configuration warnings. |
| 4 | Paste |
Paste elements that you cut or copied on the logic canvas. Keyboard shortcut to paste: Ctrl + V |
| 5 | Select |
Select an element of the logic diagram on the logic canvas to move or edit it. When you select an element of the diagram, the horizontal toolbar opens. Use this panel to edit the values in the property panel, copy, cut, duplicate, or delete an item. Keyboard shortcut to select: V |
| 6 | Pan |
See different views of the logic diagram. Keyboard shortcut to pan: H |
| 7 | Undo |
Undo the previous action on the logic canvas. Keyboard shortcut: Ctrl + Z |
| 8 | Redo |
Redo or reverse the previous undo action on the logic canvas. Keyboard shortcut: Ctrl + Y |
| 9 | Zoom In | Zoom in to the logic canvas. You can also move the wheel button on your mouse to zoom in. |
| 10 | Zoom Reset | Zoom Reset fits a logic diagram within the logic canvas. The zoom level is adjusted based on the content of the logic diagram. |
| 11 | Zoom Out | Zoom out of the logic canvas. You can also move the wheel button on your mouse to zoom out. |
| 13 | Save | Save the logic diagram. |
| 14 | Cancel | Cancel your work. |
Which logic blocks are available and what do they do?
| Logic block category | Description |
|---|---|
| Tools | Contains the Text block. Use the Text block to insert a text box in the logic diagram. See How do I add a text box to a logic diagram in the Logic Editor? for more details. |
| Input & Output | Gives you the ability to expose values from within the control logic, either as an input or output. These blocks are considered attributes of the Program (Control System) Object in which they are included. A control system is limited to a combination of 24 inputs and 24 outputs. See Table 5 for more details. |
| Constant | Passes a constant value to building block inputs. See Table 6 for more details. |
| Math | Performs mathematical functions on one or more inputs, producing a single output. See Table 7 for more details. |
| Boolean | Performs Boolean functions on two to eight inputs, producing a single output. See Table 8 for more details. |
| Statistical | Performs statistical functions on two to eight inputs, producing a single output. See Table 9 for more details. |
| Selector | Performs multiplexing for two to eight inputs, producing a single output. Based on the current mode assigned to each input, the selector chooses which input to pass through to the output. See Table 10 for more details. |
| Control | Performs control functions on three inputs, producing a single output. Most control logic blocks have three inputs. The blocks compare input number 1 with input number 2 using the differential (input number 3). The Sequencer functions differently. See Table 11 and What is a Sequencer block? for more details. |
| Psychrometric | Performs psychrometric functions on the defined inputs, producing a single output. Psychrometric logic blocks have two inputs. See Table 12 for more details. |
| Calculation | Controls the amount that an output can change per control system execution or extrapolates an output by using two inputs for reference. The Calculation category contains the Span block and Rate Limit block. See What is a Span block? and What is a Rate Limit (RL) block? for more details. |
| Timing | Passes its input to its output at the next execution of the control system, every five seconds. Timing blocks are used to break up feedback loops. See Table 13 for more details. |
| System | When you place a System block on the logic
canvas, a configuration wizard guides you through the
configuration of the control system. System blocks are useful
when you have complex logic, because they facilitate the nesting
of one control system under another control system. When you
create a System block, the Metasys software creates a Program
(Control System) Object under the first Program object in the
building network tree. Note: It is also
possible to add a child control system under a parent system
through the Network tree. However, after you add a child
system through the Network tree, you must view, modify, and
save the parent system before the child system begins
executing its
logic.
|
| Type | Description |
|---|---|
| Input Reference | After you insert an Input Reference or Output Reference, you can edit which object or attribute is being referenced. You can also launch the command dialog directly from the Logic Viewer. |
| Output Reference | |
| Input blocks: FLOAT, ENUM, and BOOL | Drag the blocks from the Logic Blocks pane to the logic canvas. Click the Property Panel icon to configure the blocks. |
| Output blocks: FLOAT, ENUM, and BOOL |
| Type | Description |
|---|---|
| FLOAT | Float |
| ENUM | Enumeration |
| REL | Release. This block sends the Release command at a specific priority based on the connection. |
|
Block |
Math function |
Inputs |
|---|---|---|
| × | Multiply | 2–8 |
| + | Add | 2–8 |
| ÷ | Divide | 2 |
| ‒ | Subtract | 2 |
| NEG | Negative | 1 |
| ABS | Absolute | 1 |
| SQRT | Square Root | 1 |
| COS | Cosine | 1 |
| SIN | Sine | 1 |
| TAN | Tangent | 1 |
| ATAN | Arc Tangent | 1 |
| ASIN | Arc Sine | 1 |
| ACOS | Arc Cosine | 1 |
| EXP | Exponent: the operation of raising to a power, whereby the power value is connected as an input | 1 |
| LN | Natural Log | 1 |
| LOG | Log | 1 |
| X^Y | X^Y | 2 |
| Type |
Inputs |
|---|---|
| AND | 2–8 |
| OR | 2–8 |
| XOR | 2 |
| NOT | 1 |
| LATCH | See What is a Latch block? |
|
Type |
Inputs |
|---|---|
| AVG | 2–8 |
| MAX | 2–8 |
| MIN | 2–8 |
| Type | Inputs |
|---|---|
| MUX | The Multiplexer block has 2–8 inputs, one mode input, and one output. Depending on the current value of the mode input, the Selector chooses which input passes through to the output. |
| Block | Statistical type | Inputs |
|---|---|---|
| > | Greater than | 3 |
| < | Less than | 3 |
| ≤ | Less than or equal | 3 |
| ≥ | Greater than or equal | 3 |
| ≠ | Not equal | 3 |
| = | Equal | 3 |
| SEQ | Sequencer | See What is a Sequencer block? |
|
Symbols |
Description | Upper input | Lower input |
|---|---|---|---|
| EnDp | Enthalpy - Dew point | DB | DP |
| EnRh | Enthalpy - Relative humidity | DB | RH |
| RhDp | Relative humidity - Dew point | DB | DP |
| RhWb | Relative humidity - Wet bulb | DB | WB |
| WbDp | Wet bulb - Dew point | DB | DP |
| WbRh | Wet bulb - Relative humidity | DB | RH |
| ABH | Absolute humidity | DB | RH |
| Dp | Dew point | DB | RH |
| Type | Description |
|---|---|
| Delay | Delay blocks have one input and one output, and are commonly used to break up feedback loops. |
| Timer | See What is a Timer block?, What is a Pulse timer?, What is an On Delay timer?, What is an Off Delay timer?, What is a Minimum On timer?, and What is a Minimum Off timer? for more details. |
| Time | See What is a Time block? for more details. |
What is a Latch block?
The Latch block holds a binary value until you command it to reset. Latch blocks help capture rapidly changing binary states that might otherwise be missed. The input of the Latch block is a binary attribute, sampled every time the logic system runs, which is every five seconds.
Reset determines if the output of the block changes with a change in the value of the input. When Reset is True, the output of the Latch block stays its original value, even if the input changes value. Reset is also a binary attribute. To change the value of Reset, click Command on the input reference block in the Logic Viewer and issue an Inactive or Active command.
This table translates the value of the input or reset binary attribute into True and False values for the Latch block:
| Binary attribute value | Command | True or False |
|---|---|---|
| 1.0 | Active | True |
| 0.0 | Inactive | False |
The following table and figure summarize the operation of the Latch block:
| Input | Reset | Output |
|---|---|---|
| Goes from False to True | False |
True Even if the Input goes to False, the Output stays True as long as Reset is False. |
| Goes from False to True | True | False |
| Goes from True to False | False |
True Even if the Input goes to True, the Output stays False as long as Reset is False. |
| Goes from True to False | True | False |
What is a Sequencer block?
Sequencer blocks activate devices in a sequential order based on the rank of the device and whether the device is enabled. Lower ranked devices are activated before higher ranked devices, and higher ranked devices are deactivated before lower ranked devices.
The input value at which the sequencer activates or deactivates each device is based on the make and break limits configured for the Sequencer. See Table 39 for information about configuring the make and break limits. The defaults for a 3-stage Sequencer with a range of 0–100 are the following:
| Make limits (activation points) | Break limits (deactivation points) | |
|---|---|---|
| Stage 1 | 33 | 1 |
| Stage 2 | 67 | 34 |
| Stage 3 | 99 | 68 |
Sequencer blocks can output a value for minimum of 2 and maximum of 8 devices. The following table describes the components of a Sequencer block:
| Component | Description |
|---|---|
| Input | Determines the number of activated stages. |
| Instant Shutdown |
Determines if the Sequencer is enabled or disabled. Use a binary object attribute (1.0=Enabled, 0.0=Disabled). |
| Rotate Now |
Activates reordering of output sequence. The manner in which the outputs Device 1 Output through Device 8 Output are reordered for activation is based on a combination of two factors: the ranking defined for each device, and whether the device is enabled. All enabled outputs are scheduled for output selection prior to disabled outputs. And, within each of these categories (enabled and disabled outputs), the selections are ordered beginning with the lowest ranked and proceeding on through to the highest ranked output. Unlike all other reordering scenarios, the issue of whether or not a device is currently active is not taken into account in this situation. Use a binary object attribute (1.0=Rotate now, 0.0=Do not rotate now). |
| Device 1–8 Enable |
Establishes whether or not the output is enabled. Use a binary object attribute (1.0=Enabled, 0.0=Disabled). |
| Device 1–8 Rank | Establishes the order in which device outputs are activated. Use an analog object attribute (reference block) or a Constant block. |
|
Binary attribute value |
Command | True or False |
|---|---|---|
| 1.0 | Active | True |
| 0.0 | Inactive | False |
What is a Span block?
The Span block applies a range and extrapolated values to an input to produce an output. This table describes the Span block components:
| Symbol | Description |
|---|---|
| IN | Input |
| IL | Input Low |
| OL | Output Low |
| IH | Input High |
| OH | Output High |
The Span block creates a linear relationship between the low input/output and high input/output pair. If the Input for the Span block falls between the low and high input, the Output of the Span block is found on the line between the low and high pairs.
The following example shows a graphical picture of how the Span block works:
The line connecting the low and high pairs (blue line) represents the linear relationship between them. When you enter an Input for the Span block, the logic finds where the line crosses that input and provides the corresponding output. The output must lie on the thick blue line. Using the previous figure, if you enter 5 for the Span block Input, the block would find 5 on the Input axis and provide an output of 5.5 because that is where the line crosses an Input value of 5. The green line shows this relationship.
If the Span block is configured to clamp the value of the Output, the Output of the block is restricted to the range between (and including) the low and high Output you enter for the block. Range clamping is the default setting. For example, assume you are using the values in the following figure and have clamping set to True. If you enter an Input of 5, you still generate an Output of 5.5, because the original line crosses an Input of 5 at 5.5, which is between 4 and 8 (low and high output). If you enter an Input of 12, you generate an Output of 8, because where the original line crosses an Input of 12 is higher than the high output (see where thin blue and thin green lines intersect). If clamping is True for both high and low, the output must lie on the newly drawn thick blue line.
The Span block works for the reverse span also, if the Output High is lower than the Output Low. See Table 42 for information about editing Span blocks.
What is a Rate Limit (RL) block?
The Rate Limit block controls the rate at which its Output changes with variations in its Input value. If rate limiting is disabled, this block passes the value of the Input to the Output. If rate limiting is enabled, this block limits changes to its Output to an increment determined by the Step Equation, executed according to the rate limit. This table describes the components of the Rate Limit block:
| Symbol | Description |
|---|---|
| IN | Input |
| EN |
Enabled Enables rate limiting. Use a binary object attribute reference for EN: 0 = Disabled (Inactive command) 1 = Enabled (Active command) |
Rate Limit blocks use the Step Equation to determine the maximum increment (step) the Output can change to match the Input if the two differ. The Step Equation recalculates the step every time system logic executes (every 5 seconds).
The Step Equation looks like this:
Step = Rate Limit/60,000 x Actual Period, where Rate Limit is the rate per minute to increase or decrease the Output until it matches the Input, and where Actual Period is the time in milliseconds since the last execution of the block. The system logic and Step Equation execute every 5 seconds (5,000 milliseconds).
For example, if the Rate Limit block is set up like this:
Rate Limit = 10
Actual Period = 5,000 (milliseconds)
The Step Equation looks like this:
Step = 10/60,000 x 5,000
Step = 0.8
So, the maximum increment the Output can change on its way to match the Input is 0.8.
What is a Timer block?
This table describes the components of the Timer block:
| Output | Description |
|---|---|
| IN | Input |
| RS | Reset. Cancels the timer. Reset does not apply to Minimum On or Minimum Off timers. Use a binary object attribute for Reset (1.0=Reset Active, 0.0=Reset Inactive). |
The LCT contains five different types of timers, including the Pulse timer, On Delay timer, Off Delay timer, Minimum On timer, and Minimum Off timer. Each type uses a duration (how long the timer is active) and unique functions to generate an Output.
What is a Pulse timer?
The following table and figures illustrate the function of the Pulse timer.
| Feature | Description |
|---|---|
| Activation | Goes active if the Input goes from low to high in two consecutive executions (logic executes every five seconds. The Pulse timer remains active for the amount of time specified in Duration, then goes to inactive. High to low transitions do not activate this timer. |
| Output | Stays high as long as the timer is active. After the Duration expires, the Output goes low at the next logic execution. |
| Reset | Cancels timer activity and makes the output low. If the Reset goes from high to low, the timer re-evaluates the Input at the next low to high transition. |
| Example | Captures a short pulse on a binary input and keeps the Output True long enough so that the logic can react to it. |
What is an On Delay timer?
The following table and figures illustrate the function of the On Delay timer.
| Feature | Description |
|---|---|
| Activation | Goes inactive in a low to high Input transition,
depending on the state of the input during the duration period. If
the Input returns to a low state (inactive), the timing cycle is
canceled and the Output remains inactive. If the Input remains in a
high state, the Output goes to the high state at the next execution
of logic. In a high to low Input transition, the Output becomes inactive the next time the logic executes (logic executes every 5 seconds). |
| Output | See previous row. |
| Reset | Cancels timer activity and makes the output inactive. If the Reset goes from active to inactive, the timer re-evaluates the Input at the next low to high transition. |
| Example | Delays the supply fan start 20 seconds after the return fan starts. |
What is an Off Delay timer?
The following table and figures illustrate the function of the Off Delay timer.
| Feature | Description |
|---|---|
| Activation | In a low to high Input transition, the Output becomes
active the next time the logic executes (logic executes every 5
seconds). Goes inactive in a high to low Input transition, depending on the state of the input during the duration period. If the Input returns to a high state (active), the timing cycle is canceled and the Output remains active. If the Input remains in a low state, the Output goes to the low state at the next execution of logic. |
| Output | See previous row. |
| Reset | Cancels timer activity and makes the output inactive. If the Reset goes from active to inactive, the timer re-evaluates the Input at the next low to high transition. |
| Example | Keeps the fan running to purge the coils after a heating or cooling system is turned off. Off Delay is useful when your building contains electrical heat and/or DX cooling. |
What is a Minimum On timer?
The following table and figures illustrate the function of the Minimum On timer.
| Feature | Description |
|---|---|
| Activation | See the following row. |
| Output | Goes active when there is a low to high Input transition when the timer executes (logic executes every 5 seconds). The Output remains active until the time specified in Duration passes AND the Input returns to inactive. |
| Reset | Has no effect on Minimum On timer. |
| Example | Keeps a chiller running for a minimum time after startup to stabilize equipment. |
What is a Minimum Off timer?
The following table and figures illustrate the function of the Minimum Off timer.
| Feature | Description |
|---|---|
| Activation | See the following row. |
| Output | Goes inactive when there is a high to low Input transition when the timer executes (logic executes every 5 seconds). The Output remains inactive until the time specified in Duration passes and the Input returns to active. |
| Reset | Has no effect on Minimum Off timer. |
| Example | Keeps a chiller off from a minimum time after shutdown to equalize refrigerant. |
What is a Time block?
A Time block has no configurable input because it extracts time and date information from the network. The time is based on the time of the engine under which the logic diagram is created and it is local time. The outputs of a Time block are six time and date values:
| Output | Description | Format |
|---|---|---|
| HH | Hour | 0–23 (24-hour time) |
| MM | Minute | 0–59 |
| YR | Year | four-digit year |
| MO | Month | 1–12 |
| DA | Day | 1–31 |
| DOW | Day of the Week |
1=Monday 2=Tuesday 3=Wednesday 4=Thursday 5=Friday 6=Saturday 7=Sunday |
How do I add a new logic block in the Logic Editor?
- From the Logic Blocks pane, select the required block.
- For example, select an Input Reference block, then drag and drop the block on the logic canvas.
- In the Attribute Name window, select the required item from the Network tree or Views and then select the required attribute from the Attribute list in the bottom-left of the window.
- Click OK.
- From the Logic Blocks pane, select the System block.
- Drag and drop the block on the logic canvas.
- In the Create Item window, enter a unique identifier and click NEXT.
- Configure the object as required and click CREATE.
- From the Logic Blocks pane, select the required block.
- Drag and drop the block on the logic canvas.
How do I add a text box to a logic diagram in the Logic Editor?
- From , select Text.
- Drag and drop the Text block on the logic canvas.
- Click on the Text block. A horizontal toolbar opens.
- On the toolbar, click the Property Panel icon.
- In the Text field, enter the required text.
How do I edit a logic block in the Logic Editor?
- Click on the logic block that you want to edit. A horizontal toolbar opens.
- On the toolbar, click the Property
Panel icon. Note: The Property Panel icon is disabled for blocks that are not configurable. The options available in the Property Panel depend on the type of logic block.
See the following tables for more details about the respective blocks that you want to edit.
| Field | Description |
|---|---|
| Name | Name of the input. Note: The name cannot begin with a hyphen (-).
The name cannot consist of only a space, or only a double
quotation mark (").
|
| Units | The units for the output. This field appears for floating inputs only. |
| Display Precision |
Tells the Metasys software what precision to use when formatting data. This field appears for floating inputs only. |
| Enum Category |
Set category determined by the user interface, either Two State or Multi State. This field appears for Enum inputs only. |
| Enum Set |
Set determined by the category selected in Enum Category. This field appears for Enum inputs only. |
| Trigger |
This is checked if you want the attribute to trigger the control system to execute if its value changes by more than the defined increment. |
| Field | Description |
|---|---|
| Label | Enter a label for the block. Note: Do not start labels with a number and then
follow it with any of these characters: $ . - , In addition,
the label cannot consist of only a space, or only a double
quotation mark (").
|
| Object | Specify the network item this block should reference. When you drag this block onto the logic canvas, you are prompted to select an object and an attribute. |
| Attribute | The attribute to which the reference is linked. When you configure an Input reference, the drop-down list contains numeric attributes only. |
| Units | Units for the attribute |
| Trigger | This is checked if you want the attribute to trigger the control system to execute immediately instead of waiting for the next control system scan if the value changes by more than the defined increment. Otherwise, the control system executes normally. |
| Increment | Sets the increment. |
| Field | Description |
|---|---|
| Name | Name of the output. Note: The name cannot begin with a hyphen
(-). The name cannot consist of only a space, or only a
double quotation mark (").
|
| Units | The units for the output. |
| Display Precision |
Tells the Metasys software what precision to use when formatting data. This field appears for floating outputs only. |
| Enum Category |
Set category determined by the user interface, either Two State or Multi State. This field appears for Enum outputs only. |
| Enum Set |
Set determined by the category selected in Enum Category. This field appears for Enum outputs only. |
| Field | Description |
|---|---|
| Label | Enter a label for the block. Note: Do not start labels with a number and then
follow it with any of these characters: $ . - , In addition,
the label cannot consist of only a space, or only a double
quotation mark (").
|
| Object | Specify the network item this block should reference. When you drag this block onto the logic canvas, you are prompted to select an object and an attribute. |
| Attribute | The attribute to which the reference is linked. When you configure an Output reference, the drop-down list contains numeric, writable attributes only. |
| Field | Description |
|---|---|
| Enum Category | Set category determined by the user interface, either Two State or Multi State. |
| Enum Set | Set determined by the category selected in Enum Category. |
| Enum | Set state determined by the set and set category. |
| Field | Description |
|---|---|
| Value | The value of the float. |
| Units | The units used by the float. |
| Field | Description |
|---|---|
| Input | The number of inputs depends on the type of block that you use. The input count cannot be lower than the number of current connections. |
| Field | Description |
|---|---|
| Input | The number of inputs depends on the type of block that you use. The input count cannot be lower than the number of current connections. |
| Field | Description |
|---|---|
| Input | The input count cannot be lower than the number of current connections. |
| Field | Description |
|---|---|
| Input | The number of inputs determines the list of inputs. |
| Enum Category | Filters the enumeration set list based on the chosen category. |
| Enum Set | When Enum Set changes, all modes are reset. |
| Input 1 Mode(s) | Click the button and a dialog box appears that allows you to select which modes associate with each input. In the dialog box, select the check box next to the desired mode(s). If a mode is already assigned to another input, the mode appears dimmed. Select Default to select all modes for an input that are not currently selected by any other input. |
| Input 2 Mode(s) | Click the button and a dialog box appears that allows you to select which modes associate with each input. In the dialog box, select the check box next to the desired mode(s). If a mode is already assigned to another input, the mode appears dimmed. Select Default to select all modes for an input that are not currently selected by any other input. There is one of these per input (2–8). |
| Field | Description |
|---|---|
| Type | The Type of comparison performed by the block. This field defaults to what was dragged over. |
| Field | Description |
|---|---|
| Outputs | Determines the number of binary outputs for the block. |
| Min On Time | Specifies the minimum time an output must be on before being deactivated to an off condition. When an output is activated, a timer starts. Until the timer reaches the minimum time, the output cannot be deactivated. However, an Instant Shutdown or a Rotate Now command is applied immediately, and overrides the Min On Time value. |
| Min Off Time | Specifies the minimum time an output must be off before being reactivated to an on condition. When an output is deactivated, a timer starts. Until the timer reaches the minimum time, the output cannot be activated. However, an Instant Shutdown or a Rotate Now command is applied immediately, and overrides the Min Off Time value. |
| Interstage On Delay | Defines the minimum time that must elapse between the sequential activation of Sequencer stages. |
| Interstage Off Delay | Defines the minimum time that must elapse between sequential deactivation of Sequencer stages. |
| Make/Break Limits |
The box next to Make/Break indicates if Proactive is selected and, when you click, launches the Make/Break Dialog box. In the Make/Break Dialog box:
Make/Break Limit Rules:
|
| Field | Description |
|---|---|
| Elevation | Configure the current elevation of the site in feet or meters. |
| Unit Type |
Choose International System of Units (SI) or Imperial (IP) units. Units for Unit Type SI are kilograms of water per kilogram of dry air. Units for Unit Type IP are pounds per cubic foot. |
| Field | Description |
|---|---|
| Rate Limit | Specifies the rate per minute to increase or decrease the Output until it matches the Input. |
| Startup Value | Specifies the value the rate limiter block will start at when the engine is restarted and block enable is true. |
| Field | Description |
|---|---|
| Clamp High | Selects whether (True) or not (False) to clamp the Output at the Output High (OH). |
| Clamp Low | Selects whether (True) or not (False) to clamp the Output at the Output Low (OL). |
| Field | Description |
|---|---|
| Startup Value | Displays the initial value of the Delay block. |
| Field | Description |
|---|---|
| Duration | Specifies the length of the timer function in seconds. The range is 5–86,400 seconds. |
| Setup | Determines the type of timer
you use:
|
| Icon | Description |
|---|---|
| Add | Click the Add icon to add one or more attributes to expose. |
| Delete | Select the check box next to one or more attributes and click the Delete icon to remove the selected attributes from the System. |
How do I copy, cut, duplicate, or delete a logic block?
- Click on the logic block that you want to copy, cut, duplicate, or delete. A horizontal toolbar opens.
- On the toolbar, hover over the icons and select the action you
want to perform. For example, click the Delete icon to
delete the logic block. Note: You can copy, cut, duplicate, or delete all types of logic blocks. Press Ctrl and select multiple blocks to copy, cut, duplicate, or delete multiple blocks at the same time.
How do I connect logic blocks in the Logic Editor?
- On the logic canvas, go to the first logic block that you want to connect.
- Move your cursor over the output port of the logic block until a + symbol appears.
- Click and drag the line to the logic block that you want to connect. Note: If the Priority Connection window opens, select the required priority. The Priority Connection window opens if you make a connection to an Output Reference block only.
What are the rules for connecting blocks?
| Component | Rules | |
|---|---|---|
| System blocks | Attribute properties:
|
Supported connection type:
|
| Math, Boolean, Statistical, Selector, Control, Psychrometric, Calculation | Connect all inputs for these Logic blocks. If you attempt to save logic that is missing inputs, a configuration warning message appears. You can save the logic anyway or supply inputs where necessary. It is best practice to save the logic with inputs. In the Logic Editor, connected block ports are filled with color. Unconnected block ports appear without any color filled in. | |
How do I re-route a connection in the Logic Editor?
- Place the cursor over an existing end connection point until the cursor
changes into a + symbol.Note: You can move the end connection point only. To completely change the connection, see How do I delete a connection in the Logic Editor?
- Drag the end connection point to the port of another block.
How do I delete a connection in the Logic Editor?
- Click on the connection line that you want to delete.
- In the Line Display toolbar, click the Delete icon. You can also use the Delete button on your keyboard to delete a connection line.
How do I hide a connection in the Logic Editor?
- Click on the connection line that you want to hide.
- In the Line Display toolbar, click Hide.
How do I run the Logic Checker?
- In the Logic Editor, click the Logic Checker icon in the upper-right corner.
- If the Logic Checker does not detect any configuration warnings, the following message appears: No issues found.
- If the Logic Checker detects configuration warnings, the following
message appears: Configuration warnings
found. Hover over the exclamation points to learn more about the
configuration warnings. The following table outlines the different
configuration warnings.Note: The configuration warnings remain until you fix the errors.
| Condition | Message text |
|---|---|
| An output is not connected. | Output not connected |
| An input is not connected. | Input not connected |
| A feedback loop exists in the logic. | A loop has been detected, the program may not run properly |
How do I create a Program (Control System) object?
For details about creating an object, see Creating and deleting objects.
How do I view and edit Program (Control System) object attributes?
To view and edit Program (Control System) object attributes, open the Detail widget of the Program (Control System) object.
Is the Logic Viewer and Editor supported on all devices?
You can use the Logic Viewer on desktop computers, tablets, and smartphones. For best performance on a tablet or smartphone, use an iOS device to view the logic diagram in the Logic Viewer. You can use the Logic Editor on desktop computers only.