What is the Equipment Serving Space widget?
Use this widget to view all equipment that directly serves a space along with any equipment upstream. With this widget, you can easily see information about a VAV, Air Handler, Chiller Plant and/or Heating Plant that serve a room.
What is the layout of the Equipment Serving Space widget?
Figure 1 and Table 1 describes the Equipment Serving Space widget in JCT.
Figure 1. Equipment Serving Space widget

Number | Name | Description |
---|---|---|
1 | Equipment name | Identifies the equipment serving the space. |
2 | Filter menu | Filters the type of equipment to display in the widget. |
3 | Additional equipment serving space | Identifies additional equipment serving the space. |
4 | Page count icon | Indicates how many pieces of equipment of the same type directly serve a space. |
5 | More button | Displays all of the display data for the piece of equipment. |
6 | Long name | Displays the long name of the point. |
7 | Short name | Displays the short name of the point. |