What is a Building Network dashboard?
The Building Network dashboard provides a cohesive summary of the selected object. The widgets included on a Building Network dashboard vary based on the type of object you are viewing. For more information, refer to sections that cover the different types of widgets.
How do I get to a Building Network dashboard?
The Space dashboard is the default view when you first log in to the JCT. To navigate to a Building Network dashboard, click the Network or Views tab. Click you object that you require.
Note: Users who do not have permission to
view the Building Network can only view the Spaces tree.
Is the Building Network dashboard supported on all devices?
Yes, the Building Network dashboard is supported on desktop, tablets, and smartphones.