What is JCT used for?
JCT is for validating spaces, equipment, and for creating and editing Metasys UI graphics, and assigning associations to all supported graphics.
JCT is installed with the SCT software and does not require a Metasys server.
JCT also provides an alternative for accessing features and functionality that are available in Metasys UI for only certain platforms.
- Create, delete, modify, and associate Metasys UI graphics using JCT's Graphics Manager and Graphics Editor.
- Manage BACnet/SC certificates using JCT's BACnet/SC Management feature.
- Configure the email server and DDA type notifications using JCT's Remote Notifications feature.
- Create, delete, modify, and associate Metasys UI graphics using JCT's Graphics Manager and Graphics Editor.
- Manage BACnet/SC certificates using JCT's BACnet/SC Management feature.
What devices, operating systems, and browsers does JCT support?
The following tables list the operating systems and browsers the JCT client supports:
|
Supported mobile phone operating systems |
Android 10.0 or later iOS® 13.0 or later |
|
Supported tablet operating systems |
Android 10.0 or later iOS® 13.0 or later Note:
|
|
Supported client computer operating systems and web browser combinations |
Windows® 11 Pro
and Windows® 11
Enterprise versions 22H2, 21H2 (64-bit) General Availability
Channel (GAC)
Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit). Windows® 10 Enterprise LTSC (1809, 21H2) (64-bit)Web browsers supported:
|
|
Apple® macOS® 11 Big Sur Apple® macOS® 10.15 Catalina Apple® macOS® 10.14 Mojave Web browsers supported:
|
|
Supported web browsers |
Google®
Chrome™ version 101 or
later
Notes:
|
| Microsoft® Edge® version 101 or later | |
|
Apple®
Safari®
15 or later
Note:
JCT does
not support Private browsing. To exit Private browsing,
click or tap Private in the
browser window.
|
|
|
General web browser support information |
|
|
Supported communication channels |
For optimal performance, use a wired connection for computers that browse to the JCT. Ethernet network interface card 10/100/1000 Mbps Wireless IEEE 802.11 connection 4G Network
Notes:
|
For more information on supported server platforms for installation of the JCT software, refer to the Metasys Server Installation and Upgrade Instructions (LIT-12012162) and SCT Installation and Upgrade Instructions (LIT-12012067).
What are the related documents for JCT?
The following table lists the related documents for JCT.
|
For information about |
Refer to |
|---|---|
|
How to install and configure the ADS, ADX, and Metasys UI |
Metasys Server Installation and Upgrade Instructions (LIT-12012162) |
|
How to install the ADS-Lite |
ADS-Lite Installation and Upgrade Instructions (LIT-12011688) |
|
How to install the OAS |
Open Application Server (OAS) Installation and Upgrade Guide (LIT-12013222) |
|
How to install the NAE85 |
NAE85 Installation and Upgrade Guide (LIT-12011530) |
|
How to install the LCS85 |
LCS85 Installation and Upgrade Guide (LIT-12011623) |
|
How to install the SCT and JCT |
SCT Installation and Upgrade Instructions (LIT-12012067) |
|
Using the Metasys UI |
Metasys UI Help (LIT-12011953) |
|
Creating Spaces and Equipment |
SCT: System Configuration Tool Help (LIT-12011964) and SCT Pro Help (LIT-12013035) |
|
Managing Archives |
|
|
Configuring Trend Extensions, Schedules, and Alarm Extensions |
Metasys UI Help (LIT-12011953) |
|
Managing Metasys UI Databases, Metasys UI System Preferences, and Troubleshooting information |
Metasys UI Technical Bulletin (LIT-12012115) |
|
Creating Custom Symbols |
Metasys UI Custom Symbols Technical Bulletin (LIT-12013054) |
| Metasys for Validated Environments (MVE) and using Metasys UI on an MVE site |
Metasys for Validated Environments on Metasys UI Product Bulletin (LIT-12014261) Metasys for Validated Environments on Metasys UI Technical Bulletin (LIT-12014262) |
Is the data shown in JCT current?
No. The widgets, the Graphics Manager, and the Graphics Editor do not display data values. In place of current data values, Point Info displays. If Point Info displays, it validates that there is a point configured for the piece of equipment.
Why does my screen look different on different devices?
The JCT adapts to the device on which it is viewed.