Frequently asked questions - Metasys - LIT-12012116 - Server - Metasys UI - 7.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
7.0
Revision date
2024-09-25

What Metasys sites support spaces and equipment?

Spaces and equipment are supported on Metasys sites that have a Metasys server as their Site Director. From Release 12.0, spaces and equipment are also supported on Metasys sites with an NAE85 or LCS85 Site Director. From Metasys 13.0, SNC and SNE engines include Metasys UI, however, spaces and equipment are not supported on Metasys sites with an SNC or SNE Site Director.
Note: Spaces and equipment are defined at the site level and do not apply at a child device level.