Alarm commands - Metasys - LIT-12012116 - Server - Metasys UI - 7.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012116
Version
7.0
Revision date
2024-09-25

The following table lists the commands supported by the alarm extensions feature.

Table 1. Alarm extension commands

Command Name

Parameters

Description

Cancel Delay Time

None

Cancel Report Delay

None

Enable None Enables the alarm extension. The extension will re-evaluate its current condition and start generating alarms and events as appropriate.
Disable None Disables the alarm extension. Until re-enabled, the alarm extension will not generate any new alarms or events.