Alarm extensions - Metasys - LIT-12012116 - Server - Metasys UI - 7.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012116
Version
7.0
Revision date
2024-09-25

An alarm extension adds alarm detection to an item. Alarm extensions monitor an attribute of an object and generate alarms and events when the attribute's value meets certain conditions, based on the extension's type and configuration. There are two types of alarm extensions: analog alarm and multistate alarm.