Extensions - Metasys - LIT-12012116 - Server - Metasys UI - 7.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012116
Version
7.0
Revision date
2024-09-25

What is an extension? Which extensions are supported in Metasys UI?

An extension adds features such as trending or alarming to an item. From Metasys Release 12.0, the following actions are supported for extensions:
Table 1. Extensions support
Extension type View and edit Create
Alarm Yes Yes
Trend Yes Yes
Totalization Yes Yes
Averaging Yes Yes
Load Yes Yes
Resource file Yes No

See Creating and deleting objects for more information about creating extensions.