Working with the Tools Tab - Metasys - LIT-12012116 - Server - Metasys UI - 7.0

Johnson Controls System Configuration Tool (JCT) Help

Product name
Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
7.0
Revision date
2023-09-01

How do I use the Import Custom Symbols option?

To use the Import Custom Symbols option, click IMPORT CUSTOM SYMBOLS. For more detailed information about the Import Custom Symbols option, see Working with Symbols.

How do I use the Export Custom Symbols option?

To use the Export Custom Symbols option, click EXPORT CUSTOM SYMBOLS. For more detailed information about the Export Custom Symbols option, see Working with Symbols.