What is the Graphics Manager?
The Graphics Manager is the single point of entry for creating and editing Metasys UI graphics, including Aliased graphics, the Master Layer graphic, and templates. The Graphics Manager allows you to view and manage space and equipment associations with all supported graphics. You can also export and import Metasys UI graphics and Custom Symbols with the Graphics Manager.
How do I access the Graphics Manager?
- Open the user menu.
- Click Feature Management.
- Click Graphics Manager.
While in the Graphics Manager, if you open the Navigation panel and select a space, you exit the Graphics Manager and are redirected to the Space dashboard of the selected space.
What is the layout of the Graphics Manager?
Number | Name | Description | |
---|---|---|---|
1 |
Graphics tab | Opens the Graphics tab. You can view graphics, create, edit, and delete Metasys UI graphics, and associate graphics with spaces, equipment, Equipment Definitions, and network objects. By default, the Graphics tab is open when you access the Graphics Manager. | |
2 |
Location list |
Equipment & Spaces |
Lists the equipment and spaces configured on the site. Click on an equipment or space to view the
associated graphics in the Graphics List and to create or edit
Metasys UI graphics for the equipment or space. In the Graphics
List, graphics associated with the equipment or space are listed
in the same order as the SCT archive and in the Graphics widget.
However, for equipment, if an Exception graphic exists, the
Aliased graphic appears in the list with an Note: This selection does not apply for
cases where the site director is an SNx engine.
|
Equipment Definitions |
Lists the Equipment Definitions configured on the site. Click on an Equipment Definition to view the
Aliased graphic and any Exception graphics that are associated
all of the equipment tied to the Equipment Definition. In the
Graphics List, Aliased graphics are listed first and Exception
graphics displaying after the Aliased graphics. An Note: This selection does not apply for
cases where the site director is an SNx engine.
|
||
Network |
Lists the network objects configured to the site. Click on a network object to view the associated graphics in the Graphics List and to create or edit Metasys UI graphics for the network object. From Release 13 engines, select the engine's Graphics folder, or any graphic in that folder, to manage Metasys UI graphics on that engine. Note: If
Network is grayed out in the Graphics tab Location list, the
required device packages are not installed or the feature is not
supported. For more information, see Installing and licensing device packages.
|
||
3 |
Graphics List | Lists the graphics for:
|
|
4 |
Graphics list toolbar | Add, copy and paste, and delete a Metasys UI graphic, or reorder the list of supported graphics. | |
5 |
Preview panel | Displays a preview of the graphic. The Preview panel
displays the first graphic in the Graphics List. Click a graphic in
the Graphics List to view a preview of the graphic. Note: The preview does not display animation or live
data.
See also Working with the Preview Panel. |
|
6 |
Graphics Editor icon | Opens the Graphics Editor with the previewed graphic open for editing. The Graphics Editor icon displays for Metasys UI graphics only. | |
7 |
Graphic details | Lists the name of the graphic, the type of graphic, and the number of items assigned to the graphic, the description, and the authorization category of the graphic. | |
8 |
View & Assign button | Click to view and assign the equipment, space, or network object associated with the graphic. | |
9 |
Tools tab | Opens the Tools tab. The Tools tab allows you to find and replace point names in Metasys UI graphics, including templates. The Tools tab also allows you to import and export Metasys UI graphics and Custom Symbols. | |
10 |
Master tab | Opens the Master tab. The Master tab allows you to create a Master Layer graphic. | |
11 |
Templates tab | Opens the Templates tab. The Templates tab allows you to view system templates and create custom templates. |
What types of graphics are supported in the Graphics Manager?
The following types of graphics are supported in the Graphics Manager:
Type of graphic | Description | Editor |
---|---|---|
Metasys UI | Any graphic created in the Metasys UI or JCT. | Graphics Editor |
Unassigned Graphic |
An unassigned graphic can be the following:
When you associate an unassigned graphic to an equipment or space, it no longer appears in the Graphics List when the Unassigned Graphics folder is selected. Note: The Graphics Manager supports up to 1500 unassigned
graphics.
|
Graphics Editor for Metasys UI graphics GGT for Graphics+ graphics UGT in SMP or SCT for Standard graphics |
Equipment Graphic |
A Metasys UI graphic associated with a piece of equipment. An Equipment graphic can also be an Exception graphic. An Exception graphic is a Metasys UI graphic associated with a piece of equipment that already has an Aliased graphic associated with its Equipment Definition. When a piece of equipment has one or more Exception graphics, the Aliased graphic is disabled. | Graphics Editor |
Space Graphic |
A Metasys UI graphic associated with a space. | Graphics Editor |
Aliased Graphic |
A Metasys UI graphic that is created for an Equipment Definition. By default, an Aliased graphic displays on every Equipment dashboard in which the equipment references the associated Equipment Definition. If an Exception graphic is also associated with the equipment, the Aliased graphic does not display and is disabled for that equipment's Equipment dashboard. | Graphics Editor |
Exception Graphic |
A graphic that displays on a subset of associated equipment's Equipment dashboard instead of the Aliased graphic that is associated with the equipment's Equipment Definition. An Exception graphic is typically used when equipment differs from the other equipment associated with an Equipment Definition (for example, equipment with different ductwork). An Exception graphic can be a Metasys UI graphic, Graphics+ graphic, or a Standard graphic. |
Graphics Editor for Metasys UI graphics GGT for Graphics+ graphics UGT in SMP or SCT for Standard Graphics |
Custom Template |
A Metasys UI graphic that is a user-defined graphics template. | Graphics Editor |
Graphics+ Graphic | A legacy graphic created in the Graphic Generation Tool and associated with spaces, equipment, or field controllers. |
Graphic Generation Tool (GGT) |
Standard Graphic | A legacy graphic created using the UGT in SMP or SCT and associated with spaces, equipment, or field controllers. |
UGT in SMP or SCT |
How do I work with the Graphics Manager?
To view graphics, create and edit Metasys UI graphics, and associate graphics with spaces, equipment, network objects, and Equipment Definitions, see Working with the Graphics Tab.
To view system templates and custom templates, see Working with the Templates Tab.
To view, create, and edit the Master Layer graphic, see Working with the Master Tab.
To find and replace short names in Metasys UI graphics, export Metasys UI graphics or Custom Symbols, or import Metasys UI graphics or Custom Symbols, see Working with the Tools Tab.
To manage the associations between a graphic and spaces and equipment, see Working with the Preview Panel.