What are the available VRF Systems symbols?
|
1 Way Cassette |
4 Way Cassette |
|
Wall Mounted |
Ducted High Static |
|
Outdoor Unit |
Changeover Box |
What are the properties available for VRF Systems symbols?
All VRF System symbols have no Property panel properties, except the Outdoor Unit symbol. The Outdoor Unit symbol allows you to select the Number of Outdoor Unit from One to Four units.
The following VRF System symbols have the same Binding properties: 1 Way Cassette, 4 Way Cassette, Wall Mounted, and Ducted High Static.
The Outdoor Unit symbol has different Binding properties and the Changeover Box has no Binding properties.
| Binding | Short Name | Animation Available |
|---|---|---|
| Unit Status | UNT-S | No |
| Unit Operation Mode | N/A | Yes |
| Fan Status | FAN-S | Yes |
| Fan Speed | FAN-O | No |
All VRF System symbols have no Snapping Properties.
What are the Binding properties available on the Outdoor Unit symbol?
| Binding | Short Name | Animation Available |
|---|---|---|
| Outdoor Unit 1 Primary Value | OU1-S | Yes |
| Outdoor Unit 1 Secondary Value | OU1-C | No |
| Outdoor Unit 2 Primary Value | OU2-S | Yes |
| Outdoor Unit 2 Secondary Value | OU2-C | No |
| Outdoor Unit 3 Primary Value | OU3-S | Yes |
| Outdoor Unit 3 Secondary Value | OU3-C | No |
| Outdoor Unit 4 Primary Value | OU4-S | Yes |
| Outdoor Unit 4 Secondary Value | OU4-C | No |