What are the available Heat Exchanger symbols?
|
Plate Exchanger |
Shell Exchanger |
|
What are the properties available on the Heat Exchangers symbols?
Both Heat Exchanger symbols have no Property panel properties.
Both Heat Exchanger symbols have the same Binding properties.
| Binding | Short Name | Animation Available |
|---|---|---|
| Input Primary Value | HX1ISOV-C | Yes |
| Output Primary Value | HX1V1-O (for Plate Exchanger)
HXMV-O (for Shell Exchanger) |
Yes |
| Input Secondary Value | N/A | No |
| Output Secondary Value | N/A | No |
| Navigation | N/A | No |
All Heat Exchanger symbols snap to Pipe symbols that are water pipes.