What are the available Air Damper symbols?
Vertical Parallel Damper |
Vertical Opposed Damper |
Horizontal Parallel Damper |
Horizontal Opposed Damper |
Horizontal Round Damper |
Vertical Round Damper |
What are the properties available for the Air Damper symbols?
All Air Damper symbols have no Property panel properties.
All Air Damper symbols have the same Binding properties.
Binding | Short Name | Animation Available |
---|---|---|
Damper Primary Value | MAD-O | Yes |
Damper Secondary Value | N/A | No |
Navigation | N/A | No |
All Air Damper symbols snap to all horizontal ducts from the Ductwork symbols.