What are the available Triggers?
The following triggers are available for Custom Behaviors: Left Click & Hold (Tap & Hold & Tap), Double Click (Double Tap), Mouse Over, and Value Change. The Tap & Hold & Tap and Double Tap triggers are available on tablet and phone platforms as well as touch-enabled computer platforms.
The following table lists the supported trigger and effect combinations. Note that when multiple behaviors or multiple effects for a single behavior are configured, the triggers available are limited.
| Trigger | Effect |
|---|---|
| Left Click & Hold (Tap & Hold & Tap) | Show Hide Change Color (Custom) Note: To start the Change Color effect on tablets or phone
platforms, tap, then hold the shape or symbol with your finger.
To end the execution of the effect, tap on the symbol again.
Flash (Custom) Note: To start the Flash effect on tablets or phone platforms, tap,
then hold the shape or symbol with your finger. To end the
execution of the effect, tap on the symbol again.
Rotate (Simple) Note: For
the Left Click & Hold (Tap & Hold & Tap) trigger
with the Rotate effect, in order to end the execution of the
effect, the mouse or your finger must be on the shape, symbol,
element of symbol, or image when the mouse or your finger
release the hold.
Tooltip Text Change |
| Double Click (Double Tap) | Tooltip |
| Mouse Over | Show Hide Change Color (Custom) Flash (Custom) Rotate (Simple) Note: For the Mouse Over trigger with the
Rotate effect, the mouse must stay at the Origin Point for the
effect to execute.
Tooltip Text Change |
| Value Change Note: A Custom Behavior with a Value
Change trigger requires at least one rule.
|
Show Hide Change Color (Custom and System-defined) Flash (Custom and System-defined) Span Transition Rotate (Simple and Span) Text Change |