Working with Multiple Behaviors and Multiple Effects - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

How do I select the execution mode of multiple Custom Behaviors or Multiple effects?

To select the execution mode after creating multiple Custom Behaviors or multiple effects, choose:
  • First Valid: Each behavior or effect executes by order from top to bottom. The first behavior is the highest priority and is executed first. The last behavior is the lowest priority and is executed last.
    Note: You can order the Custom Behaviors by dragging and dropping the behaviors in the desired order.
  • All Valid: All behaviors or effects run simultaneously if the trigger and rules are true.
    Note: If Flash, Change Color, and Span Transition are applied with All Valid execution mode, only the Custom Behavior or effect at the top of this list executes and the remainder are ignored.