What is the Space dashboard?
The Space dashboard provides a cohesive summary of the selected space, including the equipment that serves.
How do I get to the Space dashboard?
The Space dashboard is the default view when you first log in to the JCT. To navigate to a Space dashboard, tap or click a space in the navigation panel, a link to another space in a widget, or a navigation button within a graphic in the Graphics widget. You can also search for a space and tap or click the space in the search results.
When would I first see the Graphics widget on a default Space dashboard?
If a graphic is configured for a space, the default dashboard layout has the Graphics widget appear first. To see other widgets, use the page drop-down in the upper-right corner of the dashboard. The Graphics widget may not appear first, or be available at all, if a custom dashboard has been applied.
What is the layout of the Space dashboard in JCT?
The following figure and table describe the Space dashboard in JCT.
|
Number |
Name |
Description |
|---|---|---|
|
1 |
Navigation Panel: Spaces tree |
Shows the spaces tree and allows you to navigate through your spaces. |
|
2 |
Navigation Panel: Building Network tree |
Shows the building network tree and allows you to navigate through your objects. |
|
3 |
Hamburger icon |
Opens or closes the Navigation Panel. |
|
4 |
Offline indicator |
Indicates you are accessing the JCT. |
|
5 |
Equipment Serving Space widget |
Displays all equipment that directly serves a space along with any equipment upstream. |
|
6 |
Equipment Summary widget |
Lists all similar equipment that directly serves the space and all downstream spaces. |
|
7 |
Potential Problem Areas widget |
This widget does not display data in JCT. |
|
8 |
Search field |
Search for any space or equipment on your site. |
|
9 |
User menu |
Opens User menu options. |
|
10 |
Page Navigation drop-down |
Displays the page you are currently on. Click or tap on the drop-down to navigate to a different page. |
|
11 |
Point Info |
Click or tap to display point information, including the point's short name and fully qualified reference. |