What are Graphics+ graphics?
Graphics+ graphics provide a visual representation of the monitored systems, including your HVAC systems and floor plan layouts, which enable you to quickly check the status of system symbols and recognize unusual system conditions. You can create and edit Graphics+ graphics using the Graphic Generation Tool. You can save Graphics+ graphics to your computer or save them directly to a supported Metasys host, such as a Site Director, supervisory engine, or an SCT archive. To associate Graphics+ graphics to a space or equipment, the Graphics+ graphic must be saved to the Metasys host.
Graphics+ graphics are converted at runtime when viewed in the JCT.
How do I create or edit Graphics+ graphics?
You can create and edit Graphics+ graphics using the Graphics Generation Tool (GGT). The GGT is a stand-alone software application that runs on a computer with a supported Microsoft Windows operating system. You use the tool to build the graphical representations of the monitored and controlled equipment in the facility.
For general information about the GGT, refer to Graphics+ Product Bulletin (LIT-12011698) . For more information about creating and editing Graphics+ graphics, refer to Graphic Generation Tool Help (LIT-12011697) and Graphics+ Style Guide Help (LIT-12011705) .
What Graphics+ graphics can I view in the Graphics widget?
You can view any Graphics+ graphics, including floor plan graphics, air handler graphics, equipment graphics, and plant graphics. You can also view Graphics+ graphics with custom behaviors. All Graphic Enterprise Library (GEL) elements within Graphics+ graphics are viewable, except the Room Control Module and the Trend Module, in the JCT.
Some Graphics+ graphics created in the GGT version 1.1 or 1.2 have viewing issues in the JCT. For Graphics+ graphics created in the GGT version 1.1 or 1.2, you may need to open and save those graphics in the GGT version 1.3. If you do not have the GGT version 1.3 or your branch configured your graphics, contact your local Johnson Controls branch representative.
What features of the Graphics+ graphics are not supported in the JCT?
Some of the features of Graphics+ graphics are not converted or functional when viewing the graphics in the JCT.
- When saving Graphics+ graphics to the Metasys Host in the Graphics Generation Tool, do not save the graphic under the Site object. We recommend saving the graphics in a folder. Graphics saved under the Site object do not appear in the Metasys UI or JCT.
- Trend Module
- Right-click triggers for Custom Behaviors
- Show Command Dialog Custom Behavior
- Navigation to an external, mailto, or .exe files
- Color opacity set using the
- Color gradients for the following symbol types: HVAC Pumps, Pipes, Art Canvas (background), and Advanced Value Box
- Radial gradients
What features of the Graphics+ graphics display differently in the JCT than in SMP or SCT?
Some of the features of Graphics+ graphics appear differently in the JCT than in SMP or SCT.
- In Microsoft Edge, tooltips for Room Control Modules and other similar symbols may not appear consistently when a tooltip exceeds 55 characters with no special characters or spaces separating the alphanumeric characters. To resolve this issue, you may enter special characters to force line breaks in the tooltip or do not allow tooltips to exceed 55 characters.
- Basic Value Box (with show status selected in the GGT) displays the status (does not display in SMP)
- Colors of symbols may appear lighter or darker than in SMP or SCT
- For shapes drawn in the art canvas using the GGT version 1.2 library tools, the fill color displays on all overlap objects (looks different than in the SMP). However, for shapes drawn in the art canvas using the GGT version 1.3 library tools, the fill color displays as it does in the SMP.
- Expand and collapse for the Key Data Module works only when tapping or clicking the expand or collapse button.
- Some types of supported gradients (for example, linear gradients). Also, for gradients with multiple colors applied to some pipes and pumps, the first color applied only appears.
- Key Data Item highlighting
- Key Data Module is not movable
In certain instances when text does not appear or if it appears cut off in the JCT converted Graphics+ graphic, you may need to resize the text box by a few pixels in the GGT before viewing the graphic in the JCT again. After resizing the text box, saving the graphic, and displaying the graphic in the JCT, text box width is not 100% accurate or displayed the same as in SMP or SCT.
For CAD drawings and some symbols and elements of graphics with AUTO height and width settings display with missing data or appear smaller than desired. To resolve this issue, manually resize the CAD drawing, symbol, or element of the graphic so that the height and width are numeric values and not AUTO.
For pipes color accuracy, there may be slight differences in appearance on computer platforms and tablet and phone platforms.
Do I need Microsoft Silverlight® installed to view Graphics+ graphics in JCT?
No. To view Graphics+ graphics in the JCT, you do not need to install Microsoft Silverlight.
Do the Graphics+ graphics display current data values in the Graphics widget?
No. Graphics+ graphic elements that support current data values do not display current data values of the bound points in the JCT.
Can I command from the Graphics+ graphics in the Graphics widget?
No. You cannot command from Graphics+ graphics in the JCT.
Can I view aliased Graphics+ graphics from a Graphics+ graphics in the Graphics widget?
Yes. Aliases to other graphics that are associated with equipment configured JCT are supported. Refer to the Graphic Generation Tool Help (LIT-12011697) .
Where can I find more information about Graphics+ graphics?
|
For Information on |
See Document |
|---|---|
|
Using the Graphic Generation Tool and Creating Graphics+ Graphics |
Graphic Generation Tool Help (LIT-12011697) |
|
Best Practices for Creating Graphics+ Graphics |
Graphics+ Style Guide Help (LIT-12011705) |
|
Viewing Characteristics and Behavior of Graphics+ Graphic Elements |
Graphics+ Runtime Help (LIT-12011708) |
|
Associating Graphics with Spaces and Equipment |
Metasys UI Technical Bulletin (LIT-12012115) |