Graphics widget - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

My space does not have any graphics associated with it. Which graphic does the Graphics widget display instead?

If there are no graphics associated with a space, the Graphics widget displays the first equipment graphics of the first equipment that is associated with the space.

If the first equipment does not have equipment graphics associated, then the Graphics widget displays the alias graphics of the first equipment that is associated with the space.

If there are multiple pieces of equipment serving the space, the feature checks on a sequential basis for available equipment graphics or alias graphics. For example, if the first equipment associated with the space does not have equipment graphics or alias graphics configured, the feature looks for the first equipment graphics of the second equipment serving the space, and if that is unavailable, the feature looks for alias graphics of the second equipment serving the space.

Tap or click on the graphic selection drop-down menu to select a different graphic to view in the Graphics widget.

The Graphics widget displays the message No graphics are configured for this space. if none of the pieces of equipment serving the space have any equipment or alias graphics configured.

The Graphics widget may also display the message No graphics are configured for this space. after a Site Director name change. To ensure that graphics are displaying you have to click or tap Refresh All Archives in the user menu in JCT after a Site Director name change. Refer to How do I refresh the archive I am currently working on? How do I update the archive with the changes recently made? in the Using archives chapter of Johnson Controls System Configuration Tool (JCT) Help (LIT-12012116) for details about refreshing an archive.

Is the Graphics widget supported on all devices?

Yes, the Graphics widget is supported on desktop, tablets, and smartphones.