What is the Equipment dashboard?
The Equipment dashboard provides a cohesive summary of a selected piece of equipment.
How do I get to the Equipment dashboard?
To navigate to an Equipment dashboard, tap or click an equipment's name in a widget or a navigation button within a graphic in the Graphics widget. You can also search for a piece of equipment and tap or click the equipment's name in the search results.
Associated equipment object links are viewable from many places in the UI, including Alarm Manager. You can navigate to equipment through these links, if you have access.
When would I first see the Graphics widget on an Equipment dashboard?
If a graphic is configured for a piece of equipment, the default dashboard layout with the Graphics widget appears first. To see other widgets, use the Navigation page drop down in the header of the Metasys UI. The Graphics widget may not appear first, or be available at all, if a custom dashboard has been applied.
What is the layout of the Equipment dashboard in JCT?
The following figure and table describe the layout of the Equipment dashboard in JCT.
Number |
Name |
Description |
---|---|---|
1 |
Navigation Panel: Spaces tree |
Shows the spaces tree and allows you to navigate through your spaces. |
2 |
Navigation Panel: Building Network tree |
Shows the Building Network tree and allows you to navigate through your objects. |
3 |
Hamburger icon |
Opens or closes the Navigation Panel. |
4 |
Offline indicator |
Indicates you are accessing the JCT. |
5 |
Trend widget |
This widget does not display data in JCT. |
6 |
Equipment Activity widget |
This widget does not display data in JCT. |
7 |
Search field |
Search for any space or equipment on your site. |
8 |
User menu |
Opens User menu options. |
9 |
Page navigation drop-down |
Displays the page you are currently on. Click or tap on the drop-down to navigate to a different page. |
10 |
Point Info |
Tap or click to display point information, including the point's short name and fully qualified reference. |
11 |
Equipment Data widget |
Displays all points within the selected piece of equipment. This widget does not display the current point values in JCT. In Metasys UI, the Equipment Data widget displays the current point values. |
12 |
Equipment Relationships widget |
Displays all relationships a piece of equipment has with other equipment, spaces, and network field controllers. This widget does not display online or offline status in JCT. In Metasys UI, the Equipment Relationships widget displays online or offline status of the equipment listed. |