JCT icons - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

The following table lists the icons that appear on the home screen of the JCT.

Table 1. JCT general navigation icons
Icon Icon name Icon description
Hamburger Opens or closes the navigation panel, which includes the Spaces tree and the Building Network tree.
Search Opens the search field.
User menu Opens user menu options.

The explanation for the icons related to widgets and specific features is in the section where the widget or feature is described.