How do I access and log in to the JCT?
To access the JCT on a device (computer or mobile device), ensure that you have access credentials to the Metasys System Configuration Tool (SCT).
In a supported web browser, navigate to https://[host name]/UIOffline, where [host name] is replaced with the host name, server name, or IP Address of the SCT computer. If you are on the SCT computer with JCT installed, you can also navigate to hostname/UIOffline or localhost/UIOffline.
When browsing to the JCT, your web browser displays a security certificate warning. The browser displays this warning if your JCT site does not have a trusted security certificate.
- For Google Chrome :
- Tap or click Advanced.
- Tap or click Proceed to [IP Address], where [SERVERNAME or IP Address] is the server name or IP address of the SCT computer. The JCT login screen appears.
- For Windows Internet Explorer 11 or Microsoft Edge, tap or click Continue to this website (not recommended). The JCT login screen appears.
- For Apple Safari 8 or later, tap or click Continue in the Cannot Verify Server Identity window. The JCT login screen appears.
We strongly recommend installing a trusted security certificate. For more information about installing trusted security certificates, refer to Network and IT Guidance Technical Bulletin (LIT-12011279) and contact your IT department.
When the JCT login screen appears, enter your SCT login credentials.
Can I log in with my Active Directory® account?
You can log in using your Active Directory user name and password if the Active Directory login feature is set up in the SCT. For more information about Active Directory and the Metasys system, refer to Network and IT Guidance Technical Bulletin (LIT-12011279) .
Can I log in with my Office 365® account?
You can log in with your Office 365® user name and password if the Office 365® login feature is set up in the Metasys system. For more information on Office 365® and the Metasys system, refer to the Network and IT Guidance Technical Bulletin (LIT-12011279) .
How do I log out?
To log out of the JCT, tap or click the User menu icon in the upper-right of the screen, then tap or click Log Out.
Why should I log out?
To make sure your JCT site remains secure, always log out of the JCT.
Why am I asked to accept the terms and conditions?
All new Metasys users are required to accept the Terms and Conditions of use before they access the Metasys system for the first time.
Why did my session expire? Why was I logged out without clicking the Log Out button?
After 30 minutes of inactivity, your session automatically terminates and you are returned to the login screen. The default timeout is 30 minutes. If your tablet or phone goes to sleep or you lose connection, you are logged out and returned to the login screen. See the Session Inactivity and Other Settings section for more information.