What is the navigation panel?
The navigation panel is located on the left side of the screen and facilitates the navigation through the Spaces and Network tabs.
Can I resize the navigation panel?
Yes, you can resize the navigation panel on a computer platform by dragging the double-headed arrow. The panel retains the resizing when you navigate to the Graphics Manager, for example, but the resizing does not persist on logout.
How do I open or close the navigation panel?
To open or close the navigation panel, click the hamburger icon.
What is a space?
Spaces help you organize the information displayed for the Metasys system into physical locations (a campus and its buildings) and areas within those locations (floors, zones, and rooms). The hierarchy resembles the physical world to help you navigate your Metasys system. Each space has a hierarchical relationship to other spaces, as well as a served-by relationship to the equipment that provides services to the space. For more information on how to configure spaces and equipment, refer to the SCT: System Configuration Tool Help (LIT-12011964) .
How do I navigate through the hierarchy of the trees?
The navigation panel shows the list of spaces, point objects, and extensions objects that have been configured to organize the information in your Metasys system. To navigate to a specific room, select the highest level in your Spaces tab. For example, first select your building, then your floor, then finally your room on that floor. To navigate to a network object, click the Network tab. For example, to navigate to an IP controller, first expand the relevant engine and then the relevant BACnet Integration object. To navigate to an object in your assigned User Views, click the Views tab, select the relevant User View from the list, if there are more than one, and navigate to the required object.
How do I get back to the space or object I was previously at?
To navigate to a previous space, use your browser's back button or use the navigation panel. You can also navigate to a previous space or object by clicking on the hyperlink in the breadcrumb hierarchy.
How do I bookmark a location to return to later?
Invalid Space ID
message appears on the screen and you are re-directed to the root space.
Mobile devices:
- To bookmark a location on an Android device, navigate to the location that you want to bookmark, tap the bookmark icon, select Add Bookmark, name your bookmark, and tap Save.
- To bookmark a location on an Apple device, navigate to the location that you want to bookmark, tap the bookmark icon, select Bookmark, name your bookmark, and tap Save.
Icon | Icon description |
---|---|
|
Bookmark icon on an Android device. |
|
Bookmark icon on an Apple device. |
Desktop or laptop devices:
- To bookmark a location in Google Chrome, navigate to the location that you want to bookmark, click the bookmark icon with the tooltip Bookmark this tab, click Add bookmark name your bookmark, and click Done.
- To bookmark a location in Apple Safari, navigate to the location that you want to bookmark, click Bookmarks, select Add Bookmark, name your bookmark, and click Add.
- To bookmark a location in Microsoft Edge, navigate to the location that you want to bookmark, click the bookmark icon with the tooltip Add this page to favorites, name your bookmark, and click Done.
Icon | Icon description |
---|---|
|
Bookmark icon in Google Chrome. |
|
Bookmark icon in Microsoft Edge. |
How do I return to a previously bookmarked location?
Browse to the bookmarked location from your browser's list of bookmarks.