Totalization commands - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

The following table lists the commands supported by the Totalization extensions.

Table 1. Totalization commands

Command name

Parameters

Description

Disable

None

Enable

None

Reset

None

Reset Rollover

Access level = Supervise