Analog totalization - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

The Analog totalization extension tracks and records the usage of any consumable monitored through an analog attribute. Some examples of consumables include electricity, gas, steam, and chilled water.

These three essential parameters determine the Analog totalization extension’s mode of operation:

  • the Input Reference to be monitored
  • the Timebase on which the computation is based
  • the Low CutOff Value that the input must meet or exceed

Use the Analog totalization extension to determine the usage of the given consumable. For example, you can determine the amount of gas or steam used by the facility for a given month. Also, use Analog totalization to determine how many kilowatt/hours were used in a week or to totalize a calculated value (for example, degree days).

The Analog totalization extension contains attributes common to Metasys system objects. The following table lists the attributes specific to the Analog totalization extension.

Note: In the Notes column, the letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
Table 1. Analog totalization extension attributes

Attribute name

Notes

Initial value

Values/Options/Range

Description

Display Precision

C,W

10ths

Uses Display Precision (Set 0)

Executing

 

Active

Active

Totalize Limit

Inactive

Active: The extension is calculating and has not reached the Totalize Limit.

Totalize Limit: The extension has reached the limit and has stopped calculating because Rollover is set to False.

Inactive: The extension is unreliable or disabled and is not calculating.

Input Reference

C

   

Low CutOff Value

C,W

   

Present Value

C,D,R,W

   

Reliability

 

Reliable

Uses Reliability (Set 503)

Reset (This attribute does not appear in a view, but may be scheduled, trended, and so on.)

W

False

False

True

Reset Date

     

Reset Time

     

Rollover

C,W

False

False

True

Rollover Count

 

0

0–4,294,967,295

Scale Factor

C,W

1.0

Minimum Value > 0

Timebase

C,W

Hours

Seconds

Minutes

Hours

Totalize Limit

C,N,W

 

Limit > 0

Units

C,W

 

IP

SI

Value Before Reset