Load rating - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20
Note: Enter Energy Savings amounts in decreasing order, with the highest amount listed first. Enter the same Shed to value in all rows.

Consider an example of a fan that should be shed to 60%. The first Shed from entry is 100%, because the most energy would be saved when shedding from this state. The second Shed from entry is 90%, the third entry is 80%, and so on.

Also, consider an example of a three-speed fan that can have the following states: High, Medium, Low, and Off. The operator decides to set the fan to Low when the Load is shed. In this case, the first Shed from entry is High because the most energy would be saved when shedding from this state. The second Shed from entry is Medium. A Shed from entry for Off is not required because no energy is saved by shedding from Off to Low. The entries might look like this:

Table 1. Load rating entries

Shed from

Shed to

Energy savings

High

Low

5.0 kW

Medium

Low

3.2 kW