Analog alarm extension examples - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document type
User Guide
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

The analog alarm extension adds the alarming capability for attributes with real values, such as the Present Value of an Analog Input Object. This extension detects an alarm in two different modes: the Single Setpoint method, or the Cooling/Heating Setpoint Method.