Alarm extensions - Metasys - LIT-12012116 - Server - Metasys UI - 6.0

Johnson Controls System Configuration Tool (JCT) Help

Product
Building Automation Systems > Graphics and Interfaces > Metasys UI
Document number
LIT-12012116
Version
6.0
Revision date
2022-05-20

An alarm extension adds attributes for generating alarm and event messages to an item. Alarm extensions monitor an attribute of an object and send alarms using the Alarm Manager. There are two types of alarm extensions: analog alarm and multistate alarm.