How do I access the Tools tab?
You can access the Tools tab from the Graphics Manager. The Tools tab is available in the Metasys UI and the JCT.
What are the options available in the Tools tab?
- GLOBAL FIND & REPLACE: Find and replace exact point short names in all Metasys UI graphics, including custom and system templates, equipment graphics, space graphics, Aliased graphics, and the Master Layer graphic.
- IMPORT GRAPHICS: Import Metasys UI graphics from a .export file (previously exported Metasys UI graphics).
- EXPORT GRAPHICS: Export Metasys UI graphics to a .export file.
- IMPORT CUSTOM SYMBOLS: Import custom symbols.
- EXPORT CUSTOM SYMBOLS: Export custom symbols.
How do I use the Global Find & Replace option?
To use the Global Find & Replace option in the Tools tab, click GLOBAL FIND & REPLACE. For more detailed information about the Global Find & Replace option, see Using Global Find and Replace.
How do I use the Import Graphics option?
To use the Import Graphics option, click IMPORT GRAPHICS. For more detailed information about the Import Graphics option, see Using Import Graphics and Export Graphics.
How do I use the Export Graphics option?
To use the Export Graphics option, click EXPORT GRAPHICS. For more detailed information about the Export Graphics option, see Using Import Graphics and Export Graphics.
How do I use the Import Custom Symbols option?
To use the Import Custom Symbols option, click IMPORT CUSTOM SYMBOLS. For more detailed information about the Import Custom Symbols option, see Working with Symbols.
How do I use the Export Custom Symbols option?
To use the Export Custom Symbols option, click EXPORT CUSTOM SYMBOLS. For more detailed information about the Export Custom Symbols option, see Working with Symbols.