What is the Graphics tab?
The Graphics tab allows you to view graphics, create, edit, and delete Metasys UI graphics, and associate graphics with spaces, equipment, network objects, and Equipment Definitions. By default, the Graphics tab is open when you access the Graphics Manager.
How do I work with the Graphics tab?
The following actions are available in the Graphics tab:
- You can view supported legacy graphics and any unassigned Metasys UI graphics. For more information, see Working with the Graphics List and Working with the Preview Panel.
- You can create, edit, copy and paste, and delete Metasys UI graphics. For more information, see Creating Equipment, Space, Network, or Unassigned Graphics.
- You can create, edit, copy and paste, and delete Aliased graphics. Aliased graphics can only be Metasys UI graphics. For more information, see Creating Aliased Graphics.
- You can create, edit, copy and paste, and delete Metasys UI Exception graphics, as well as view supported Metasys UI legacy graphics. For more information, see Creating Exception Graphics.
- You can view and assign associations to supported legacy graphics and any unassigned graphics. For more information, see Working with the Preview Panel.