What are the available Water Sensor symbols?
|
Well Temperature Horizontal |
Well Temperature Vertical |
|
Well Temperature Horizontal Left |
Well Temperature Horizontal Right |
|
Well Temperature Vertical Type 2 |
Temp Strap On |
|
Differential Pressure Horizontal |
Differential Pressure Vertical |
|
Pressure Single Horizontal |
Pressure Single Vertical |
|
Flow Orifice Horizontal |
Flow Orifice Vertical |
|
Flow Paddle Wheel Horizontal |
Flow Paddle Wheel Vertical |
|
Flow Switch Horizontal |
Flow Switch Vertical |
|
Flow Ultrasonic Horizontal |
Flow Ultrasonic Vertical |
|
Flow Venturi Horizontal |
Venturi Vertical |
|
Horizontal Level Switch |
Ultrasonic Level |
|
Alphasonic Level |
Vertical Level Switch |
|
Pipe Heat Tape Horizontal |
Pipe Heat Tape Vertical |
|
Condensation Sensor Horizontal |
Condensation Sensor Vertical |
|
Air Compressor |
Emergency Push Button |
|
Deaerator |
Vessel |
What are the properties available on the Water Sensor symbols?
All Water Sensor symbols have no Property panel properties.
The Deaerator symbol has no Binding properties.
| Symbol | Snaps To |
|---|---|
| Well Temperature Sensor Vertical | Pipes: Diagonal and Diagonal End water pipes |
| Well Temperature Horizontal Left
Well Temperature Horizontal Right |
Pipes: Vertical and Vertical End air-side pipes |
| Well Temperature Vertical Type 2
Ultrasonic Level |
Pipes: Diagonal, Diagonal End, Continuation Pipe, Horizontal, Horizontal End, and Horizontal Continuation Pipe air-side pipes |
| Pressure Single Vertical
Flow Orifice Vertical Flow Paddle Wheel Vertical Flow Switch Vertical Flow Ultrasonic Vertical Flow Venturi Vertical Pipe Heat Tape Vertical Condensation Sensor Vertical |
Pipes: Diagonal, Diagonal End, and Diagonal End Continuation pipes |
| Pressure Single Horizontal
Flow Orifice Horizontal Flow Paddle Wheel Horizontal Flow Switch Horizontal Flow Ultrasonic Horizontal Flow Venturi Horizontal Pipe Heat Tape Horizontal Condensation Sensor Horizontal |
Pipes: Horizontal, Horizontal End, and Horizontal End Continuation pipes |
| Deaerator | Pipes: Horizontal End and Vertical End pipes |
What are the Binding properties available on the Well Temperature Horizontal, Well Temperature Vertical, Well Temperature Horizontal Left, Well Temperature Horizontal Right, and Well Temperature Vertical Type 2 symbols?
| Binding | Animation Available |
|---|---|
| Well Temperature Primary Value | No |
| Well Temperature Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Temp Strap On symbol?
| Binding | Animation Available |
|---|---|
| Temperature Primary Value | No |
| Temperature Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Differential Pressure Horizontal and Differential Pressure Vertical symbols?
| Binding | Animation Available |
|---|---|
| Differential Pressure Primary Value | No |
| Differential Pressure Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Pressure Single Vertical and Pressure Single Horizontal symbols?
| Binding | Animation Available |
|---|---|
| Pressure Single Primary Value | No |
| Pressure Single Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Flow Orifice Horizontal and Flow Orifice Vertical symbols?
| Binding | Animation Available |
|---|---|
| Flow Orifice Primary Value | No |
| Flow Orifice Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Flow Paddle Wheel Horizontal and Flow Paddle Wheel Vertical symbols?
| Binding | Animation Available |
|---|---|
| Flow Paddle Wheel Primary Value | No |
| Flow Paddle Wheel Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Flow Switch Horizontal and Flow Switch Vertical symbols?
| Binding | Animation Available |
|---|---|
| Flow Switch Primary Value | No |
| Flow Switch Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Flow Ultrasonic Horizontal and Flow Ultrasonic Vertical symbols?
| Binding | Animation Available |
|---|---|
| Flow Ultrasonic Primary Value | No |
| Flow Ultrasonic Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Flow Venturi Horizontal and Flow Venturi Vertical symbols?
| Binding | Animation Available |
|---|---|
| Flow Venturi Primary Value | No |
| Flow Venturi Secondary Setpoint | No |
| Navigation | No |
What are the Binding properties available on the Horizontal Level Switch and Vertical Level Switch symbols?
| Binding | Animation Available |
|---|---|
| Level Switch Vertical Primary Value | No |
| Level Switch Secondary Value | No |
| Navigation | No |
What are the Binding properties available on the Ultrasonic Level symbol?
| Binding | Animation Available |
|---|---|
| Ultrasonic Level Primary Value | No |
| Ultrasonic Level Secondary Value | No |
| Navigation | No |
What are the Binding properties available on the Alphasonic Level symbol?
| Binding | Animation Available |
|---|---|
| Alphasonic Level Primary Value | No |
| Alphasonic Level Secondary Value | No |
| Navigation | No |
What are the Binding properties available on the Pipe Heat Tape Horizontal and Pipe Heat Tape Vertical symbols?
| Binding | Animation Available |
|---|---|
| Pipe Heat Tape Primary Value | No |
| Pipe Heat Tape Secondary Value | No |
| Navigation | No |
What are the Binding properties available on the Condensation Sensor Horizontal and Condensation Sensor Vertical symbols?
| Binding | Animation Available |
|---|---|
| Condensation Sensor Primary Value
or Condensation Sensor Vertical Primary Value (for Condensation Sensor Vertical) |
No |
| Condensation Sensor Secondary
Value or Condensation Sensor Vertical Secondary Value (for Condensation Sensor Vertical) |
No |
| Navigation | No |
What are the Binding properties available on the Air Compressor symbol?
| Binding | Animation Available |
|---|---|
| Air Compressor Primary Status | No |
| Air Compressor Secondary Command | No |
| Navigation | No |
What are the Binding properties available on the Emergency Push Button symbol?
| Binding | Animation Available |
|---|---|
| Emergency Push Button Primary Value | No |
| Pipe Heat Tape Secondary Command | No |
| Navigation | No |
What are the Binding properties available on the Vessel symbol?
| Binding | Animation Available |
|---|---|
| Vessel Primary Level | No |
| Vessel Secondary Value | No |
| Navigation | No |